Hello Team,
We received the below question from one of our customers on the DAC101C081 device:
The datasheet of the DAC101C081 mentions a typical ZCO of 1.3 mV at VA = 3V and Iout = 200uA. I’ve measured this value on a device in typical circumstances and VA = 3.3V, Iout = 250 uA and its value is 14 mV.
So, I believe this is a mistake in the datasheet, it should be 13 mV instead of 1.3mV. This is also in line with the short-circuit current of -52 mA, and more probable considering a ZCO at TA=5V of 7.0 mV.
Please, could you advise?
Kind Regards,
Mo.