This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS1018 Single-end configuration

Guru 16770 points

Other Parts Discussed in Thread: ADS1018

Hi

We are about to use ADS1018 with single-ended input configuration.

ADS1018 has 12bit resolution, however, does it offer 11bit resolution for single-end input?

Bestregards

  • Hi na na 78,

    You are correct.  As the input measurement is differential, you lose one bit in single-ended mode as you are only using 1/2 of the range.

    Best regards,

    Bob B

  • Hello,


    Thank you for posting in TI E2E forum.

    The resolution of the ADC will always be 12 bits. However, in your case, since you are doing single-ended measurements, you are utilizing only one-half of the entire full-scale range. This is equivalent to reduction in the effective number of bits by 1.

    Giving you an example, in the full-scale range setting (±2.048 V), irrespective of whether you do single-ended or differential measurements, your resolution (or LSB size) for ±2.048 V full-scale range will always be (2*2.048)/(2^12) = 1 mV.

    Let me know if you have any questions.

    Regards,

    Krunal