This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

EEG Schematic review

Other Parts Discussed in Thread: ADS1299, OPA376, ADS1298

Hi Team:

Could you help me to check the EEG schematic? Whether it can work? I am not familar with it. Need your help on it. Thanks a lot.

ADS1299.pdf

  • Hey Derek,

    There are a few problems with this circuit. First, R18 and C20 will not have the desired effect of setting the gain for the Bias amplifier. Look at Figure 52 in the datasheet for an example connection. Second, pin 64 should be left as an open circuit. Finally, the SRB pins are connected as inputs to an op-amp, but the SRB pins are high impedance inputs to the ADS1298. This means the inputs to the OPA376 will be floating which will result in undesirable behavior. What are they trying to accomplish with the op-amp?

    Regards,
    Brian Pisani