Other Parts Discussed in Thread: ADC32RF45
Product is ADC32RF45 EVM with supporting software.
Was successful in setting up and running the initial configuration suggested for board checkout. When pursuing a change of sample rate and configuring for full rate LMF8224 mode, I get a reasonable spectrum and signal. However, at multiples of Fs/8 the signal is notched. For us this is Fs=2 GHz and the notches are 250, 500 and 750 MHz. DDC's etc are disabled.]
Steps to recreate problem: Configure the EVM for a 2 Gsample clock, using synthesizer, filtering and splitter as recommended in your TI up instructions. Use LMF 8224 mode, 14 bit full rate transfer (I used the two supporting cfg files provided with the download: LMK_ADC32RF45_LMF_8224_ExtClock.cfg and ADC32RF4X_14bit_LMFS_8224.cfg). Set the capture software device selection to ADC32RF45_LMF_8224. ADC Signal input is from 250 MHz to 750 MHz @ approximately -1 dBFS in. Signal power reported is close to the -1 dBFS mark EXCEPT for 250, 500 and 750 MHz, which are variable between -60 and -50 dBFS. The notch effect disappears by +/- 100 kHz on either side of these frequencies. This suggests a digital effect to me. Anyone have any ideas on what is causing this or can suggest some things to look for?