Dear Community,
I'm dealing with the question, if it's possible to use the Data output Clock from the ADS5400 as the master Clock for an FPGA.
How is it done on the TSW1200 Board? I see a crystal on the TSW1200 Board(U10) - is this the Master CLK for the FPGA?
I think the FPGA can't work if the Data Clock from the ADC is for example reset by a reset pulse?!
I'm very thankful for answers concerning the question, if it's possible to clock an FPGA with the Data clock from the ADC. . .
Regards,
Michael