This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS1262 Gain error calibration method

Other Parts Discussed in Thread: ADS1262

Dear sir,

Based on the ADS1262 datasheet,  on page 8,   we can get the Noise/4 level of gain error after calibration.  it's very good. 

But my question is that how to set-up the known-input- voltage to the analog input  pin of ADS1262 when do gain calibration,  can you tell me the your test signal source equipment name?

Thanks a lot!

Regards,

Jack

  • Hi Jack,

    The typical "Noise/4" gain error specification assumes an ideal full-scale input calibration signal.  The factor of "1/4" comes from statistics; the ADC averages 16 conversions, so the level of the noise will be about sqrt(16) or 1/4 the typical RMS noise performance. Obviously, if the calibration signal is inaccurate than the calibration will also provide inaccurate results...

    For PGA gain of 1 V/V, you ought to be able to use the reference voltage for the input signal since it will be exactly 100% full-scale. Otherwise, any stable input signal near (under) full-scale could work, so long as it's known (perhaps this voltage is measured back by an HP/Keysight 34401A multi-meter). Otherwise, if the calibration is taking place in the field, you'll have to rely on the accuracy of your on-board reference source.

     

    Note: You can account for a signal smaller than full-scale, when performing gain calibrations, by using the method I described here:

    Best Regards,
    Chris