This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS1018-Q1 Reference design

Guru 16770 points
Other Parts Discussed in Thread: ADS1018-Q1, ADS1018

Hi

We are about to use ADS1018-Q1 under the following condition.

Power Supply : GND - 5V

SPI 750kbps

Chip select : Low

Input : 0-5V single-end 3ch

Do you have a reference design using ADS1018 that we can refer?

Or, we appreciate if you could tell us some points that should be cared to design the circuit.

BestRegards