This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADC required 5MSPS or highr

Genius 3300 points

Other Parts Discussed in Thread: ADS804, OPA691

Hi,

1. i have a application where I need a parallel adc at 5MSPS or higher with 12 bit or higher.
2. Input voltage range: +-5V
3. Interface: parallel
4. Interface microcontroller voltage: 3.3V
5. Supply: Good if it can be powered from single positive supply. Like in Max1300 we can give only single supply but can measure bipolar.((OPtional)). Otherwise I can give bipolar supply also.

6. External buffer/opamp:  Better if not required. Otherwise I can add