Hi
I will design a DAQ board. A performance of ADC is required over 16bit/2MSPS. This is first time to me. So I have a hard time to design.
I am searching some components. I found ADS1605/1606. But EVM of them is discontinued. So I found another component ADS8412 EVM. I know the way of interface(ADC EVM → 5-6k interface card → DSP EVM). I saw that C6713 is DSP to easy interface to ADS1605/1606. But it is also discontinued. So I have some questions.
I want to select DSP that is easy to interface with ADS8412 EVM(or another EVM). Requirement : The DSP(and DSP Starter Kit) is not discontinued and have some example codes to easily interface with ADC, DAC, communication etc.
2. I use C2000series; TMS320F28335, TMS320F28069 etc. So if ADS8412 can be interfaced with the C2000 DSP, I want to use the DSPs. Is it possible and easy to interface with ADS8412 and F28335 or F28069?
If you know one of two answers, reply please.
Thanks to read.