This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADC12D1600 max input power

Genius 12865 points


Hello Team,

please confirm that my calculation regarding the maximum input power is correct:

According Chapter 6.1. Absolute Maximum Ratings (page 13) I can apply 2.5V to Vin+/- and if I limit the current to 50mA note (2) I calculate a maximum input power of 10 x log (2.5V * 50mA / 1mW) = 21dBm.

Thanks and Best Regards,

Hans