Other Parts Discussed in Thread: AFE4300, AFE4300EVM-PDK
Hello,
I have recently purchased a AFE4300_EVM REV B board and the board works well with AFE4300 Device GUI provided by TI.
So, first of all, I have tried to control the board with my serial program about a reset command. As a result, the board didn't respond to the reset command.
Below are the test conditions.
1. my serial setting (57600 baudrate / data 8 bit / No parity / stop 1 bit / hardware flow control : none ) : serial open OK.
2. For Reset command, I sent '0x72 0x73 0x74 0x3F' according to 4150.Message Communication Protocol - AFE4300EVM-PDK.pdf. : there is no response.
For reference, I checked if the reset command packets (0x72 0x73 0x74 0x3F) are outputted correctly with an oscilloscope. I think the h/w is ok.
Could you help me solve this situation ?
In addition, is the latest version of a firmware AFE4300EVMPDKFWSRC-1.0 ? If no, I'd like to get the final version.
Thanks in advances.
Elio