Other Parts Discussed in Thread: ADS1298
Good Evening,
I am having an issue with occasional data corruption when reading out data using the RDATAC mode.
I am using channels 2, 3 and 7, with the remaining channels turned off. Per the datasheet, unused channels should be read out as all 0's.
But every so often, these channels will read out with random data, and the data on other channels is also corrupt, I can see this on the output data plots.
I've verified the SPI timings, varied the SPI clock from 200K to 1M. I've verified the power supply rails.
I've seen this behavior on two different boards.
Does anybody have any thoughts.
Thanks,
TwilightEngineer