Other Parts Discussed in Thread: ADS1293
Hello,
I am using ADS1293 in my project to collect ECG signal. The microcontroller(PIC) is communicating with the ADS1293 through a 3 pin(SCLK, SDO, SDI) SPI interface. I am also using an I/O pin as CS. Through the SPI, I am writing the control registers within the ADS1293. But looks like these registers are not getting written. Through oscilloscope, I can see the control words are getting out of the microcontroller but whenever I read the same registers from the ADS1293, they are not same. I am using 4MHZ as the SCLK frequency. Can you please, tell me what is wrong here. Regards.
Nazrul