Hello,
I have a problem about my board and code. I want to receive I and Q value in I/Q mode from AFE4300.
I also did check and set the IQ_MODE_ENABLE register, DEVICE_CONTROL2 register, BCM_DAC_FREQ register and ADC_CONTROL_REGISTER2 register.
Using the reference register which is 703 ohm, I received Q value higher than 3.0 at 16, 32 and 64 khz. However, sometimes it is less than 3.0..
I think its value shold be less than 3.0. (Because that value was less than 3.0 in GUI) But my value is not...What is the problem? any idea?
Thank you,