Other Parts Discussed in Thread: ADS8509, ADS7809
Hey y'all,
My name is Terra and I am an R&D Engineer at Los Alamos National Labradors.
I'm combing through some datasheets for the ADS7809 and its immediate succesor the ADS8509. Overall solid datasheet. However, I am having issues figuring out what the maximum power/ current draw on the "VANA" pin is (i.e. how much power/ current does the analog supply draw. TI gives typical current draw on the analog at 100 kHz, and the maximum total draw of both the digital and analog cores combined, both good stats, but our analog core and digital core are powered by two supplies. The regulator providing the ADC analog supply can only put out 20 mA, hence the concern for just the analog's maximum current draw. Furthermore, our sample rate is much lower than 100 kHz and operates at a temperature lower than the maximum operating temperature of the part, so it would be nice to know maximum power draw as a function of temperature and sampling frequency. I've looked for a simulation of this part for TINA, LTSPICE, and PSPICE, but alas to not avail, but it really is only this aspect of the part that is of concern.
Any help is mega appreciated.
Thanks,
Terra