Other Parts Discussed in Thread: DAC3162EVM, DAC3162, CDCP1803, DAC3164
I'm using a DAC3162EVM in stock configuration (so, transformers enabled) and a TSW1400 board to control it. I am using the latest HSDC GUI (4.20). No matter what I do, I can't seem to get a waveform to output on channel A (J2, IOUTA2), though anything I send to channel B (as measured on J3, IOUTB2) is fine.
Moreover, whatever I see on J2, IOUTA2 tends to be a distorted, noisy version of whatever I am programming to channel B. If I set all channel B samples to zero, then channel A just seems to "float". Much like both channels do after a power cycle and before FW is loaded on the FPGA.
I have tried 2 different TSW1400 boards and 2 different DAC3162EVMs. Nothing seems to help. I have examined both EVMs and verified they are configured as per the schematic rev B from slar057.zip.
I'm clocking the DAC3162EVM with an external 250 MHz clock. Power is from an external 5V supply, and the EVM pulls 150 mA.
I'm examining the signals on J2 and J3 using a digital scope with 50 Ohm termination.
I need some help; out of ideas at this point.
Thanks,
Cliff