This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS7865 - 470nF capacitance at REFout and REFin

Other Parts Discussed in Thread: ADS7865

Hi all

Would you mind if we ask ADS7865?

There is some discription about 470nF capacitance at REFout and REFin on the datasheet.

<REFIN>
The converter generates reference, the internal reference buffer requires a rail-spikes on the reference input voltage because of to-rail input and output.
Such buffers typically contain internal switching.
Therefore, an external capacitor to two input stages; when the input voltage passes the the analog ground (AGND) should be used to mid-range area,
a transition occurs at the output stabilize the reference input voltage

<REFOUT>
A minimum of 470nF is required to keep the reference stable (see the previous discussion of REF IN ).

Is this 470nF used for smoothing or buffering mainly?

Kind regards,

Hirotaka Matsumoto