Other Parts Discussed in Thread: AMC1204
Hi,
What will happen if AMC1204 (or any similar isolated sigma delta modulators) sees input voltage that are within CMRR and absolute max voltage, but differential voltage is greater than +-250mV? Will its output bit stream be clamped at 100% of 1s/0s or will it exhibit some weird behavior?
I'm asking this because I intend to use it as over current protection device, and hence in case of a fault, its differential input voltage can be as high as 1.5V (0.25V and 1.75V on in+ and in-).
Thanks,
Bo Gao