This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Capturing Data on TSW1400 + High-speed ADC EVM

Hi,

Could you tell me the availability to save A-to-D sampling raw data such as ".csv" or ".txt"  to PC via TSW1400?

If it is available, please let me know the length of data that can be saved.

Best Regards,

Sonoki / Japan Disty

  • Hi,

    TSW1400 can save up to 512 Msamples of 16bits.  If you have multiple channels this will be split per channel.  Keep in mind the USB2/SPI interface is fairly slow when transferring the data from the TSW1400 to the PC - for a full buffer capture it may take up to 20 mins.  For the normal user which only uses 64ksamples, the transfer time is not noticeable.

    HSDC Pro allows you to save CSV data in the File - Save I32 Codes as CSV.  You can also save the Bin file which will help with larger capture sizes.

    Ken.