Other Parts Discussed in Thread: ADS1252
Hi,
I would like to ask you some questions about "Power-up" timing specifications of ADS1252.
Data sheet describes about "power-up sequence" as below, data sheet page9.
*****
Prior to power-up, all digital and analog-input pins must be
LOW. At the time of power-up, these signal inputs can be
biased to a voltage other than 0V, however, they must never
exceed +VDD.
Once the ADS1252 powers up, the DOUT/DRDY line pulses
LOW on the first conversion; this data is not valid. The sixth
pulse of DOUT/DRDY is valid data from the analog input
signal.
*****
I understand that,
During power-up(+Vdd, from 0V to 4.5V), all inputs (+Vin, -Vin, CLK, Vref, SCLK) must be lower than +Vdd (+Vdd>all inputs)
Is my understanding correct?
Or all inputs must be lower than 0.8V(digital), 0.5V(analog, Vref) during +Vdd reaches to 4.5V ??
I would like to confirm the meaning of "LOW".
And do you have the power-up timing specifications between +Vdd and all inputs signals?
Because there is no "Reset" pin with ADS1252.
I think to reset ADS1252 is only "power-up" sequence. It is important to know the timing to reset correctly.
(Please let me know if you know how to reset after power on.)
As I ask you this question, my customer has a problem about abnormal behavior of ADS1252 when powered-up.
After power-up, ADS1252 sometimes does not work (output data is always 0xFFFFFF).
In case of happenning this situation, ADS1252 begins to work by "power-down and power-up" again.
I suppose this is due to there is something input voltage at some inputs of ADS1252 during power-up.
Could you tell me any advice about this?
Thank you and Best Regards,