Other Parts Discussed in Thread: DAC5688
Hello,
My customer have a question about DAC5688.
[Q]
Which of the following is correct ?
(A) If aflag_sel=1, then rising edge of TXENABLE is used to determine the A sample. If aflag_sel=0, then the MSB of the input opposite of incoming data is used.
(B) If aflag_sel=1, then the MSB of the input opposite of incoming data is used to determine the A sample. If aflag_sel=0, then rising edge of TXENABLE is used.
(A) is written in datasheet P.36 INTERLEAVED BUS MODE (Figure 37).
(B) is written in datasheet P.22 description of aflag_sel.
Best Regards,
Hiroshi Katsunaga