I have two questions regarding the capture buffer.
1. Is it possible to fill the capture buffer in several chunks by
pulsing the Write Enable (WEN) signal?
I would like to digitize the analog input only when the input level is above
a certain limit, say 5 mV. So I would connect the output of a fast
comparator to the WEN pin.
2. The meaning of the section 'Coordinating Read Enable (REN) and
Write Enable (WEN)' in page 39 of the datasheet is nor clear to me.
What happens if WEN and REN are asserted at the same time? Does WEN
superseeds and REN is simply ignored, or does this freeze the capture
buffer operation until a RESET is applied?