This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DAC part for 10MHz Square waveform generator

Hi,

My customer is looking for a DAC that can output square waveform with 10MHz and slew rate=0.5V/nS, Output voltage level 5Vdc(pk-pk).

application: motor driver

Could you help on this? Very thanks. 

Regards,

Brian

  • Brian,

    This kind of speed is outside of the slew rate or settling time performance of a Precision Data Converter, our fastest parts are closer to 1us or 500ns settling time, you need something closer to 50ns settling time to meet these needs. I suggest you check with the High Speed Data Converters folks.