This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Min sampling rate and device clock of ADS54J60

According to Table 9:When DCM is not used,LMFS=4211,Min sampling rate is 250Msps.

while the recommended device clock is 500MHz~1000MHz, 250Msps Min sampling rate and 500MHz Min device clcok are mutually contradictory(device clock = sampling rate),

so what Min sampling rate and device clock are(no DCM)?

  • Min hu,

    We are currently working on revising the data sheet and one of the parameters that will change is the recommended device clock frequency range to 250MHz-1000MHz. This updated data sheet should be available in a couple of weeks.

    Regards,

    Jim