Hi Colleagues,
Is it possible to use the ADS1118 with a K-Type thermocouple until 1100°C? On the appnote http://www.ti.com/lit/an/sbaa189/sbaa189.pdf there is a table that goes up to 500°C. Is there a reason to this?
Regards,
Jon
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Colleagues,
Is it possible to use the ADS1118 with a K-Type thermocouple until 1100°C? On the appnote http://www.ti.com/lit/an/sbaa189/sbaa189.pdf there is a table that goes up to 500°C. Is there a reason to this?
Regards,
Jon
Jon,
Thank you for your query.
Yes, you can use a K-Type Thermocouple until 1100°C without any issues. I do not see a reason why the reference design show table and output results till 500°C only.
Thanks,
Krunal