Hi,
So I have an AFE4300 device (actually were using the AFE4300_EVM board). I would like to share the VSense electrodes with another TI AFE device.
However it looks like the AFE4300 has a an input impedance many orders of magnitude lower than the other TI AFE device. When the two are connected together, the second TI AFE input signal is too low for it to function.
The AFE4300_EVM has provision for some additional op-amps in the Vsense path.
Could anyone tell me if the additional op-amps on the AFE4300_EVM are for the purposes of electrode sharing, or is there another way I could overcome this issue.
Thanks
Stomp!