This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Powering AD5360 only with DVcc, without Vdd and Vss

Hi,

I am using AD5360 in my design. The module contains various power supplies such as +3.3V (DVcc), +15V (VDD) and +-15V (VSS). +15V and -15V is used only this interface. Can I Power On the module with only +3.3V (without +15V and -15V) for testing other interfaces of the module?


Powering the AD5360 device with DVcc alone has any adverse effect??

Kindly advise.

Surya