I have a customer asking if there is any way to daisy chain the ADS7953-Q1.
I do not see this as a possibility after looking at the data sheet, but is there any way that the serial data can be passed through using the SDI/ SDO path through the device?
He stated the following:
Often the SPI interface is a shift register (image) which automatically passes the SDI data to the SDO output while CS is active and reads/writes to the register when CS comes inactive. This allows daisy chain operation.
I do not see this as a possibility from the information given in the data sheet, but I promised the customer that I would ask.
If you have a design that could connect the ADS7953-Q1 in a pseudo-daisy-chain connection can you please send it?
Thanks for your help with this!
Richard Elmquist