Greetings,
I wonder if there is a minimum pulse width requirement on the clock provided for ADC128S102QML-SP to ensure its correct functional operation. In our current implementation using an FPGA to interface with ADC128S102QML-SP, during the assertion of CS/ there is a glitch of a few nanoseconds generated at the end of 64 clocks generated for the ADC128S102QML-SP SCLK. Will this narrow glitch cause the ADC128S102QML-SP internal control logic to become deadlocked and fail to properly function in the subsequent conversion?
Thank you.