Other Parts Discussed in Thread: AFE4300EVM-PDK, AFE4300
I have been calibrating my AFE4300 using the AFE4300EVM-PDK according to the guidlines in the PDF: Impedance Measurement with AFE4300. However when calibrating the phase offset (using the method described in section 2.2 on page 4 of the PDF) I hit a problem.
I am only interested in making measurements using the I/Q mode at a DAC DDS frequency of 64000 Hz. However, when I tried to measure the phase offset using the AFE4300EVM-PDK on board resistors, I measured a different offset for each resistance.
For the 100R resistor I measured a phase offset of 22 degrees (I = 0.00981V, Q = 0.00394V)
For the 200R resistor I measured a phase offset of 17 degrees (I = 0.01831V, Q = 0.0056V)
For the 750R resistor I measured a phase offset of 9 degrees (I = 0.06189V, Q = 0.01493V)
For the 1000R resistor I measured a phase offset of 9 degrees (I = 0.08161V, Q = 0.02097V)
Shouldn't the phase offset be constant irrespective of resistance? It looks like there is some stray capacitance somewhere. Am I doing something wrong? Which offset to I subtract from my phase measurement when I test an unknown impedance as described in section 2.2 on page 4 of the PDF?
Thanks,
Mark.