Hello
I need help with selecting a clock distribution device to support the following signals:
My input is 1920MHz (could be also 960MHz if needed)
I need to generate the following clocks:
FPGA: 80MHz LVDS or LVPECL
3XADC34J23 sampling clock 80MHz
3XADC34J23: Sysref What frequency do you recommend?
Timing IO: 80MHz LVDS or LVPECL
DAC3482 Sysref - What frequency do you recommend?
DAC38J84 Sysref - What frequency do you recommend?
No need for PLL/jitter cleaner - my signal is very clean
Low power and small size is critical - if it's better to use two parts please advise
Very important: The clock to the FPGA must be active without any digital settings sent to the device, since there is no FPGA without the clock (the chicken or the egg issue)
Many thanks