I have a customer asking the following questions:
I have a question in regards to ADC channel requirements. Does it require bonded mode interface?
I would like to know if the TI ADC will require a certain amount of lane to lane data skew. I really need skew to be consistent between power up or resets also.
My question regards to RX channel-to-channel skew tolerance of the TI ADC. Just an example, I have used ADC12D1600, but I would like to provide channel bonding guidelines on FPGA TX channels. Our JESD204B IP allows users to select bonded or non-bonded option. When bonded mode is selected, skew among the FPGA TX output signals (I, Q and clk) are constant after reset / power up cycles. When non-bonded mode is selected, there won’t be a constant skew relationship between the TX channels. By looking at block diagram of ADC12D1600, I cannot find see any de-skew block. I was looking at ADC12D1600 data sheet 6.15 Timing Requirements section earlier, and found Figure 4. Clocking in Non-Demux Mode DES Mode showing the info, somewhat similar info I was looking for. However, this diagram is based on assuming there is no skew between DI and DQ signals.
I was not sure how to answer these questions so I decided to see if you understood what the customer was talking about.
Thanks for your help with this!
Richard Elmquist