My customer can't write any code to data register of DAC8760 with setting programmable slew rate register. PLS give them any advise to solve it. The procedure to write the code is shown in below.
1. Set reset register to 1.
2. Wait 1ms.
3. Write 0x7000 or 0x0000 to configulation register.
4. Write 0x1011 to control register. SREN is set to 1 in this step.
5. Write 0x2AAA or 0x1999 to data register.
6. Read back status register after waiting for a while. The status register value is 0x0004 or 0x0000. It means SR_EN is not 1.
7. Read back data register. The code is 0x000c. It's not wirtten value in step 5 in above. It should be 0x2AAA or 0x1999.