Use the ADS1220 to measure the weight with a 4-wire load cell (10KG).
At this time, I want to transmit the output data at 2000sps using RS-232. What is the minimum specification of microcontroller?
Is it possible to review PIC16F1938?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Use the ADS1220 to measure the weight with a 4-wire load cell (10KG).
At this time, I want to transmit the output data at 2000sps using RS-232. What is the minimum specification of microcontroller?
Is it possible to review PIC16F1938?
Hi Chunho,
Welcome to the forum! It is rather difficult to determine the minimum micro requirements as I have no idea what else will be done within the micro to process. The ADS1220EVM uses an MSP430F5528 running with a clock frequency of 25MHz. This micro also has a USB peripheral set up as a virtual COM port. This combination is able to capture data at 2000sps and transmit through the USB COM to the PC.
Best regards,
Bob B