Hello
I'm Alber as FAE in Arrow Korea.
My customer will use ADC12J4000 at 20x decimation & DDR & non-P54 mode.
Accoring to Datasheet page 40, there was wrote about 'Legal K Range' is 8-32.
But on the configuraion file of ADC12J4000 EVK Tool(ADC12J4000_DB20_DDR.cfg), there was applid that KM1 value is '5'.
Which number was right number & range?
ADC12J4000
0x0021 0x00 // Initiate reset of all registers
0x0021 0x01 // De-assert reset
0x0030 0x00 // SYSREF receiver and processor off
0x0040 0x04 // Set serializer pre-emphasis for high speed PCB
0x0066 0x03 // Foreground calibration mode with timing optimization enabled
0x002B 0x13 // Change reserved register to proper setting
0x0208 0x07 // Change over-range processing to longest interval
0x0051 0x84 // Calibration optimized for large signals
0x0201 0x96 // Scrambler on, KM1 = 5, DDR, JESD disabled
0x0200 0x16 // 6.02dB gain, decimate-by-20
0x0202 0x40 // P54 PLL off, Differential SYNC, Normal data mode
0x0201 0x97 // Scrambler on, KM1 = 5, DDR, JESD enabled
0x0050 0x0E // Initiate a foreground calibration