Hello,
I would like to implement a unique system to capture heart signal and respiration signal both using the same two electrodes. What I would like to ask if what exactly I need to start: I'm sure I have to interface the front end to a microcontroller (which could be the MSP430). I'm not able to solder the two components in a pcb but there are any boards I can use maybe to link them in a breadboard? I would interface the two components by SPI. It would be ok?Then, Where I can write the firmware? Visual Studio Code would be ok? There are some already existing library I can use to develope my idea? Thank you very much