Hello,
I have a few quick questions about the AD7961 in the self clocked mode, could you please answer these questions below:
1) If you are using AD7961 in the self clocked mode can you adjust the clock frequency?
2) In my application I would prefer to use the self clock mode but the typical clock period is 4 ns, does the ADC always run at this clock speed ?
3) The max frequency however is around 8ns if you do the calculation in Table 3 note1 which would be perfect. Does the ADC adjust the clock frequency based on the time between conversions?
Thanks in advance,
Samuel