This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

small size adc card

Other Parts Discussed in Thread: ADS7953, ADS1278, ADS1178

Hi all

I need a small size (approx 50mm by 150mm)  ADC card with atleast 16 analog channels on it. Each channel sampling rate must be 48 Ksamp/s/ch and ADC resolution must be 16-bit atleast. Further more this ADC card is needed to contineuosly send 16 channel digitized data on 10/100 Mb ethernet real time (without any delay) for further processings. Max Input  voltage range is +/- 3 V. In worst case a compromise can be made on sampling rate (min samp rate 15 Ksamp/s/ch)

I search a lot for such ADC card but could not find it so i think i have to design it myself. Using some TI ADC Ic and some ethernet module can it be possible to design such complicated adc card? Kindly help me to find a solution

THANKS

  • Hi Asim,

    We don't have anything 'off the shelf' with all the features you are looking from within our group.  We do have some 16 channel parts, but not with the 16-bit resolution and speed you are looking for.    You can get 16 channels and the resolution/speed you need by using two ADS1178 or two ADS1278 devices with their discrete output mode of operation.  If you can live with 12-bits, the ADS7953 may be of interest to you as well.