Hi everybody,
We are selecting a 4 to 20 mA output dac.
We need to compare DAC161S997 with AD5421C.
The data sheet of AD5421C reports a TUE measured with internal reference and from -40 to +105 °C.
The TUE reported in the DAC161S997 data sheet is measured @ 25°C.
Questions:
1)does it include the errors of the internal voltage reference?
2)how should I calculate the TUE from -10 to +40 °C? Is it enough to calculate and sum the offset drift and the gain drift according to RSS, or are there other contributions?
3)If the answer to the first question is no, where do I find the initial error and the temperature drift of the internal voltage reference?
Thank you for any help.