Other Parts Discussed in Thread: AFE4404EVM, AFE4404
Hello all,
As a starter with the AFE4404EVM, I expected a heartbeat signal like in the documentation when the sensor is placed on my wrist. Instead I got a lot of noise with some small sign of a heartbeat. The board seems to work but my impression is that the configuration is totally wrong. I am using the SFA7050.
Some tests I've done: placing the sensor above 3 different colour papers resulting in DC outputs of the sensor. led 1 sensor gives max at the green paper, led 2 max at the red paper and led 3 is high at white. Adjusting the current through the leds has the expected effect. All logical for me so far.
Using autoconfiguration is switching off led 2 and led 3 (set to 0 mA).
I know, I can adjust all registers but I expect that the configuration as delivered is ok. So I assume something is wrong.
I am using Windows10 pro
The end application is measuring heartbeat and if possible saturation at birds (preferably small birds while flying). The first step is measuring my own heartbeat and so on. The next step is a sensor interface.
Any suggestions and help is very much appreciated.
Kind regards,
Theo van Lieshout