This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Which TI module can I use to interface an inductive sensor output to a Microprocessor digital input

Hello friends,


I was searching for a module that sits between an inductive sensor output that pulses between 5 to 150 Hz and converts this pulse into a digital input such that
the input is high when there is a pulse and low when there isnt one.

The inductive sensor is

http://files.pepperl-fuchs.com/selector_files/navi/productInfo/edb/189354_eng.pdf

I cannot redesign my existing board so I need a module/evaluation board to achieve the above. I was looking at the MSC1210 module but I am not sure if it does the job for me. Looking forward to your suggestions.


regards

Ankit