Other Parts Discussed in Thread: ADS1178, OMAP-L137
Hi
I work on a OMAP-L137 starter kit with only one ADS1178. The ADS1178 is set as following: fCLK = 27MHz, fSCLK = fCLK, CLKDIV = 1, MODE = 0, FORMAT[2:0] = 001(SPI with TDM in Fixed mode) , PWDN1~PWDN8 = 1. When using only one ADS1178, DIN pin should be tied low (on page 18 of ADS1178 Data Sheet ). But the DIN pin is not connected in the starter kit and is floating. So the ADS1178 in my starter kit will work on a "dummy daisy-chaining" condition, and the "data" shifted in using DIN appear on DOUT1 after all channel data have been shifted out even if there is no any valid data input through the DIN pin actually? I mean whether the data are shifted out on DOUT1 pin in this way:CH1~CH8—>DIN( together 24 channels in the configuration)—>CH1~CH8—>DIN—>CH1~CH8—>…… (not in this way :CH1~CH8—>CH1~CH8—>…… )? This confused me.
Regards
Liang