I have application that the ADC sampling rate change versus time. The sampling rate change from 250MHz to 450 MHz versus time with maximum variation rate of 600MHz per micro-second. Does ADC12D500RF work in this situation?
Thanks.
Bing,
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I have application that the ADC sampling rate change versus time. The sampling rate change from 250MHz to 450 MHz versus time with maximum variation rate of 600MHz per micro-second. Does ADC12D500RF work in this situation?
Thanks.
Bing,
Hi Bing
The ADC12D500RF can work with a variable frequency clock, as long as the following constraints are met:
I hope this is helpful.
Best regards,
Jim B