Other Parts Discussed in Thread: ADS1118
1 single ended sampling mode
Between the two sampling, I need to do how much delay?
During debugging, i found that the delay is less, after switch from one channel to another channel, the value of the sample is same to the value which is sampled from the previous channel.
2 about the differential sampling mode
The full scale range and the size of the corresponding LSB as shown above.

When the difference mode is used to sample the voltage between two points, the voltage difference between the two points is 0.420V.
When I change the rang from the 6.144V range down to lower the scale, i found that using the smaller range, the measured value would far from the 0.420V, and even very far away from 0.420V.
I can not understand the point, so i need to pay attention to what when i use the differential sampling mode?
3 Can you provide differential sampling and single sampling code.