Other Parts Discussed in Thread: ADS805
Greetings People. I am using two ADS805 devices, each in the configuration shown in figure 7 in the data sheet (Single ended DC coupled input between 0 and +5V). My sample clock is running at 5MHz. The problem is the parts are claiming a DC offset. I shorted both parts' +in pins to ground. One device is showing 0x10f and the other one is showing 0x118. This corresponds to 331mV and 343mV. Has anybody else seen this?
Thanks for looking at this.
Len