Hello,
We develop a application a high precision voltage measurement application. Goal is to measure voltage on an isolate side, to convert this value to a digital and transmit data over optical fiber. Then, on non isoled side, after reception we re-construct the analogue signal again. Target is to re-construct the a signal with the minimum phase and amplitude error. Signal Bandwidth is 10 to 10KHz.
On another project we use ADS1282 converter. An idea was to use directly the modulator output (3 wires) and connect it to the DAC1280. Dac1280 has only one bit stream input. Is direct connection (ADS1282 to DAC1280) possible or need we obligatory a µP between ?
Have you some application note about using the ADS1282 3 wires modulator output ?
What is the phase( or time setting) of a delta sigma converter ?
Thanks for your help
Michel