Dear Sir,
I am trying to use AFE4403 EVM for some static photoelectric measurements, checking light intensities through solvents with different concentrations. Results seem ok but I noticed that there are DC drifts and Low frequency noises (0.x to 2 Hz) on the ADC output voltages. The DC drift was small (around 1-2 mV in 30 secs with Rf = 1M ohm, Second Stage Gain of 4 ) but would affect accuracy of my measurements significantly. I just wonder if possible to reduce/remove these dc drifts and low frequency noises.
Regards,
Brian