Hello,
Is the SYSREF input signal considered as a LVDS signal or not ?
Thanks
Laurent
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Laurent,
I just received word back from the design team on SYSREF. We will be updating the limits for SYSREF input to:
Spec Min Typ Max Unit
Common Mode 0.7 0.95 1.3 V
Diff Swing 0.2 0.7 1.0 V
You should be able to connect SYSREF directly to a LVDS output (with 100 ohm termination at the end of the line) as long as you can keep the common mode less than 1.3V. Please let me know if this answers your question.
Thanks,
Dave