Other Parts Discussed in Thread: AMC7812B
Hi Team,
- In AMC7812B datasheet, maximum output data valid time is 20ns.
Is this same with any SPI clock frequency?
For example 6.25MHz and 50MHz SCLK valid output maximum time is same? - When measure rise/fall time, did we measure with 10% - 90%, 20% - 80% or VIH/VIL threshold?
Thank you.
Best Regards,
Jade
Is this same with any SPI clock frequency? For example 6.25MHz and 50MHz SCLK valid output maximum time is same?