Hi,
I'm planning to use the TSW1406EVM pattern generator together with the TSW3070EVM for a application were I need to generate short burst of arbitrary waveforms. The clock to which everything should be synchronized is ~76MHz. Synchronized to this clock I want to generate every 1 ms a short burst 40ns to 100ns of different arbitrary waveforms with 0-1V (mostly it will be a step waveform with step spacing according to 76MHz). The timing of the 1 ms, as when to start the waveform generation should be synchronized to an external signal. Can this be achieved in this configuration, as I didn't see in the manuals any inputs I could use to supply some kind of trigger signal.
Thank you in advance,
T